Other Parts Discussed in Thread: TPS53319, SN65HVD96
Hi Team,
Customer is evaluating SN65HVD82 solution for RS485 power over bus. (www.ti.com/.../tida-00527)
Now customer used 10u and 1mH on the circuit. The power is the 12V from the DC source. TPS53319 Vin connect to the right side.
Please refer to the block diagram in the bottom. Customer test the baud rate for 3MHz and 5MHz. 3MHz is not stable.
Customer has question for the HW design. could you help for the following questions?
1. what is the recommended baud rate on the BUS for stability? 1MHz, 3MHz or 5MHz?
2. What is the recommended inductor and cap value for this design?
Thanks,
SHH