Part Number: DS90UB926Q-Q1
Hi All,
We are using DS90UB926 with ds90ub921 device. setup as below,
Camera--> ds90ub921(18-bit) --> FTP link --> ds90ub926(18-bit) --> host processor
If both devices are connected with out any camera data, we could see lock LED on UB926 is ON.
But, the moment when we are giving the camera data with pclk of 80Mhz, lock LED blinks continuously and we are not getting proper output from UB926 device.
Where could be the issue on ub921 or ub926? can someone help me to solve this.
Configuration for UB926
0x01 0x04
0x03 0x4c
0x08 0x18
0x10 0x18
Configuration for UB921
0x12 0x04
Regards,
Manoj