This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: Compatibility with DS90UB940

Part Number: DS90UB953-Q1

It's not mentioned on the preliminary datasheet but will the DS90UB953 be backward compatible with the DS90UB940 or will we need to upgrade our receiver module with a DS90UB954? From the preliminary datasheet the DS90UB953 appears to have a 1-Lane FPD Link III output. If compatible with the 940 will there be a method to use the full throughput capacity i.e. using two DS90UB953 devices or will that require an upgrade to the DS90UB954?