Other Parts Discussed in Thread: TPS65982
Hello, I basically would like a SMALL host receptacle to use on my PCB design to interface with cameras and other USB2.0 and USB3.0 devices. I came across USB C receptacle, which looks really small and should work for what I need. I have a few questions:
1. Should I bother with USB C or are there other small connectors that will work?
2. What are the connections that I need? I noticed that USB C requires two SuperSpeed(SS1 and SS2) interfaces. Can I just connect the same SuperSpeed interface into both ports on the receptacle? It would be nice to be able to use the reversible feature of this connector. Also, can I do the same with the non SuperSpeed ports?
| Pin | Name | Description | Pin | Name | Description | ||
|---|---|---|---|---|---|---|---|
| A1 | GND | Ground return | B12 | GND | Ground return | ||
| A2 | SSTXp1 | SuperSpeed differential pair #1, TX, positive | B11 | SSRXp1 | SuperSpeed differential pair #2, RX, positive | ||
| A3 | SSTXn1 | SuperSpeed differential pair #1, TX, negative | B10 | SSRXn1 | SuperSpeed differential pair #2, RX, negative | ||
| A4 | VBUS | Bus power | B9 | VBUS | Bus power | ||
| A5 | CC1 | Configuration channel | B8 | SBU2 | Sideband use (SBU) | ||
| A6 | Dp1 | Non-SuperSpeed differential pair, position 1, positive | B7 | Dn2 | Non-SuperSpeed differential pair, position 2, negative[a] | ||
| A7 | Dn1 | Non-SuperSpeed differential pair, position 1, negative | B6 | Dp2 | Non-SuperSpeed differential pair, position 2, positive[a] | ||
| A8 | SBU1 | Sideband use (SBU) | B5 | CC2 | Configuration channel | ||
| A9 | VBUS | Bus power | B4 | VBUS | Bus power | ||
| A10 | SSRXn2 | SuperSpeed differential pair #4, RX, negative | B3 | SSTXn2 | SuperSpeed differential pair #3, TX, negative | ||
| A11 | SSRXp2 | SuperSpeed differential pair #4, RX, positive | B2 | SSTXp2 | SuperSpeed differential pair #3, TX, positive | ||
| A12 | GND | Ground return | B1 | GND | Ground return | ||
|
|
|||||||
3. Are the Configuration Channels(CC) and Sideband Use(SBU) pins needed?
Thank you very much for your time,