Part Number: SN75976A
Dear Sirs,
My customer wants to design control board with SN75976A to replace existing end customer control board.
The configuration shows as below.
1. Any external pull high/down necessary for input and output channel?
2. customer found the input "1A" cannot back to logic low level and will keep 1~2V DC level. Once add pull down resistor on 1A, then will back to low level. Is there any modification for such issue?
3. compared with end customer existing control board and SN75976A board, the output signal DC level of SN75976A of 1B+ and 1B- will lower than around 1~1.3V. Is it normal or not?
4. testing with above configuration,
a. signal DC level from TP2 is 0 +/- 2.5V
b. replace existing Rx board with SN75976A board, the signal DC level of TP2 is 1~5V
c. if replace existing control board with SN75976A board, the signal DC level of TP2 is 1~3V
what is the reason to have the DC level on the diff. signal?
Please help to provide your comments.
Thanks.