This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320HAI: Can this part distinguish PD charger and non-PD charger?

Part Number: TUSB320HAI

Hi Team,

We need register to show the adapter support PD or not.

Can TUSB320HAI distinguish PD charger and non-PD charger?

Can 0x08 bit0 Active_Cable_Detection achieve this requirement?

Thanks

  • Hello Daniel,

        Unfortunately the TUSB320HAI is not capable to detect any PD communication, this device only supports the basic Type-C current Advertising/detection, which is USB standard, 1.5A & 3A. As well as detecting an audio & debug accessories.

    Regards,

    Diego.