Part Number: DS110DF111
Dear Support:
We have several questions submitted in this single thread. We hope that this would be easier than submitting multiple threads at the same time. Some of our questions are obvious, but please understand our desire to ensure confirmation.
Question 1 - For the 0.022uF capacitor in series between LPF_CP_A/B and LPF_REF_A/B, the evaluation board documentation shows a 0.022uF 0201 size X5R 15% capacitor. Would an NPO or X7R temperature coefficient improve the performance for -40 to +85 Celsius operating temperature?
Question 2 - Would 5% or 10% capacitance tolerances improve the performance for an -40 to +85 Celsius operating temperature?
Question 3 - For the 25MHz oscillator, the technical data sheet recommend a standard 25MHz +/- 100ppm oscillator. The evaluation board documentation shows a +/- 50ppm oscillator with a 15pF output load capacitance.
Question 4 - Would there be any CDR performance improvement or degradation if using a +/- 50ppm or +/- 100ppm oscillator?
Question 5 - Specification 6.3 Recommended Operating Conditions (Page 5) – This section states that the SMBus (SDA, SCL) recommended operating conditions as 3.0V to 3.6V. The electrical characteristics of the SDA/SCL indicate operations between 2.1 and 3.6V. If the DS110DF111 is operating in 2.5V mode, would there be issues if the SMBus (SDA, SCL) interface is operating at 2.5V operation? We understand that the SDA, SCL communications are OD.
Question 6 - Specification 6.5 Electrical Characteristics (Page 7) Propagation Delay (TPD) – Assuming the CDR is locked to the input signal, can you specify what parameters (input signal characteristics and register settings) which will produce the maximum propagation delay?
Question 7 - Specification 6.5 Electrical Characteristics (Page 7) CDR Lock Time (TLOCK1) shows 10-30ms per DS110DF111 settings, data rate, and input channel. Assuming an optimal signal or field of merit, can you specify what input signal characteristics and register setting which will produce the maximum CDR lock time. For example, which will take longer
CTLE adapt until lock or optimum with or without the DFE. In addition, CTLE requires direct register lookup due to divide by 4/8 setting.
Question 8 - Figure of Merit Type Settings (Table 22). Can you provide general guidelines on FOM settings for different types of transmission media?
Question 9 - Please confirm for register 0x2C 0x0 and 0x3 set both HEO and VEO simultaneously.
Question 10 - CTLE Settings for Adaption, Register 0x40-0x4F (Table 23). Can you please provide the characteristics of CTLE Boost String shown in Table 23 with respect to signal levels or loss and frequencies?
Question 11 - Table 18 EOM voltage range in peak-to-peak voltage does not correlate equally in magnitude to Table 26 RMS voltage levels. Is there a reason?
Question 12 - Are there any application guidelines on the EOM settings in register 0x11 [7:6] to compute a FOM for automatic adaptation of the CTLE and the DFE?
Question 13 – The DS110DF111 cannot retime the following bit rates
a) 614.4 Mb/s
b) 768 Mb/s