Part Number: SN65HVD70
Other Parts Discussed in Thread: SN65HVD37
I have a battery powered application in which need to give full duplex RS485.
1. System should be low power as battery powered
2. 3.3V vdd supply
3. Full duplex RS485
4. Length: 2 meters max
5. End application: Electronic Vehicle. So should be immune to noise.
Edit:
6. Only one master & one slave. Communication speed default 9600,8N1 . Max can go to 115200.
Based on these I think SN65HVD70 will be ok. But I am open for suggestions if better solution is available.