Part Number: TLK1501
Hi Team,
The customer is using TLK1501.
The registers configuration are as follows:
LOOPEN=0, PRBSEN=0, ENABLE=1, LCKREFN=0, TX_EN=1, TX_ER=0
For the sender, it sends a fixed 16 bit data each time. Every 1ms force TX_DV=0 and send the synchronization code 4 times.
For the receiver, it can receive the data. But occasionally the received data and the sent data are inconsistent. RX_DV=1 and this value remains the same.
But RX_ER changes between 0 and 1.
What is reason? How to solve the issue?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments