Part Number: SN65DSI86
My customer would like to know whether our device SN65DSI86 had ever worked with ARM based chip or Qualcom platform.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ray,
The device has been implemented by multiple customers using Qualcomm platforms.
Under request, we can provide a sample code that we use in Linux for OMAP to configure the DSI8x, this code executes the initial setup for the DSI8x device, we use a function to configure the DSI8x registers, this routine creates a I2C_ client structure to configure the device registers from OMAP processor (this is only a sample code, the customer needs to modify the values in the code to match the required resolution, video format, etc… ).
This sample code can be used to configure the DSi8x devices from Linux and you also can explain to the customer that the DSI interface is fully supported on the OMAP mainline Linux kernel in the following address: