Part Number: SN65C3222E
Other Parts Discussed in Thread: SN75C3222, , SN65C1167E
Dear Technical Support Team,
I have some questions about "SN75C3222" and "SN65C1168EPWR".
These devices receive overshoot(nano sec) above abolute max on system.
If you have an information of actual value not to damage device, could you share it?
Off cource, it is out of warranty.
For example, some logic ic has clamp diode, so it withstand vcc+1.0 until 10ns(absolute max is Vcc + 0.5V)
■Absolute max
SN65C3222E:VCC(MAX) = 6V
SN65C1167E:VCC(MAX) =7V
Best Regards,
ttd