This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI: Low Power Mode , Active Mode

Guru 20090 points

Part Number: TUSB4020BI

Hello,

Could you please let me know the detail(register setting or pin setting etc..) of LOW-POWER Modes and ACTIVE MODES of TUSB4020BI?

In the customer, VDD33 and VDD11 supply current is 75 mA for VDD33 and 76mA for VDD11.
I think that these current levels are active modes current but the USB device is not connected to TUSB4020BI and disconnect from the HOST(USB_DP_UP and USB_DM_UP is open for checking supply current).
Thus, I would like to know more detail of conditions for ACTIVE MODEs.

Best Regards,
Ryuji