This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982-EVM: TPS65982 Sleep Mode Issue

Part Number: TPS65982-EVM
Other Parts Discussed in Thread: TPS65982

Hello,

I have successfully used the TPS65982 to perform sourcing/sinking and PD negotiations, but I have not been able to successfully enter sleep mode. 

I have been using the application configuration tool to set the sleep and power state settings, but when I flash the device and open the utilities tool program, the registers do not reflect any of the sleep settings, and I see the device constantly pulling 5.6mA.

Can someone help me with this issue? Entering sleep mode is a critical requirement for the design in order to prevent unnecessary battery drain.

Thanks!