Part Number: TPD1S414
Hi,
In the datasheet, it stated OVP response time to nFET off is 100ns max. But Figure 7 shows differently. Which one should I follow? What is the exact threshold for complete cut off?
Thanks.
- YY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD1S414
Hi,
In the datasheet, it stated OVP response time to nFET off is 100ns max. But Figure 7 shows differently. Which one should I follow? What is the exact threshold for complete cut off?
Thanks.
- YY
Hello,
I understand what you are talking about. However if you see on Figure 7, around 70ns after the VBUS_CON goes above the 6.2V threshold (OVP limit for TPD1S414), you see VBUS_SYS going down.
At this point the FET to VBUS_SYS is completely turned off. What you are seeing with the tail that goes to 0 is the discharging of the capacitor on VBUS_SYS.
So to answer your question of when does it exact shut off is completely dependent on the size of your capacitor on VBUS_SYS side.
Also Section 8.2.2.3 of the datasheet has a good explanation of why that capacitance is there.
Regards,
Cameron