Part Number: SN65DPHY440SS
We have previously used the SN65DPHY440SS with a certain Omnivision CMOS Imager without issue (using lane 2). Recently the same circuit (different layout) was added to another board, but used Lane 0 instead, and does not work. I scoped the clock and data signals with a differential probe on each side of the SN65DPHY440SS and saw that clock looked correct on both sides, but only LP data seemed to be crossing on the output of Lane0. On the input of Lane0, I could see the HS data, but the signal was strange in that with a differential probe across DA0P & DA0N, I saw signal on three different voltage levels, centered at 750mV, 0V, and -750mV. See enclosed scope captures (each taken at different times). Any thoughts as to what is going on here?