Part Number: TMDS181
Hi,
I have a TMDS181RGZEVM and test it for the HDMI 2.0 compliance test.
The source is a 4k video graphic card and I am able to pass the compliance test.
After connected the source to TMDS181RGZEVM via a 2 meters cable some of the tests fails.
I am using I2C_En is high, <no termination>, adaptive EQ. All are default setting.
When I try to set the source termination in the eyescan tool (status control -> misc control -> transmit termination) , it will switch back to <no termination> after click <Write All>.
I try to set at the register 0xB(4:3) to 01 and 0xA(2) to 1 then click <Write all> will reset to 0 again.
1) Do you know why the termination cannot be set?
2) What we can adjust to improve the compliance test result?