This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

P82B96: About Low-level output voltage(VOL)

Guru 21045 points

Part Number: P82B96

Hi Team,

 

Our customer are evaluating P82B96 and I2C communication is normal operation.

However, they would like to know why the low-level output voltage(VOL) occurs.

 

 

We understand that VOL is the following conditions.

 

 

And, we guess that “VOL = (ON resistance of internal output driver(RON) * ISx)”.

Is my understanding incorrect?

And, could you please let us know if you have the circuit of the internal output driver?

 

Regards,

Kanemaru

  • Hello Kanemaru-san,

    This device, like many other I2C buffers, introduces a static voltage offset onto the low level of the "S" side as a mechanism for direction control. This helps in separating the transmit and receive paths, since otherwise a low level on the R input would always couple through on the T output (as if it were driven on S by another device). To avoid this coupling and allow for the directionality of the signals to be preserved, the device drives a VOL on the R output that is greater than its VIT (input voltage threshold).

    Best regards,
    Max
  • Hi Max-san,

     

    Thank you for your prompt reply.

    My understanding is as follows.

    Is my understanding correct?

    Regards,

    Kanemaru

  • Kanemaru-san,

    Yes, it looks like you understand it properly. If the S-side VOL were 0 V, then it would cause a low level to propagate onto the R output as well. You would not want this to occur when the R input is driven low.

    Here is a summary of the behavior to hopefully make things more clear:
    - If the I2C master drives the line low, the input voltage on S would be below its VIT spec. This means that the corresponding T output would go low.
    - If the "other device" in your image drives the R input low, then the S pin would be driven to its VOL level. This is above its VIT spec, though, and so the corresponding T output would not go low.

    Please let me know if this does not make sense.

    Regards,
    Max
  • Hi Max-san,

     

    Thank you for the detail information.

    I have one more question.

     

    I understand that "VOL" must be higher than "VIT".

    (I refer to the yellow line of datasheet.)

    Is my understanding incorrect?


     

    Regards,

    Kanemaru

  • Kanemaru-san,

    Yes, your understanding is correct.

    Regards,
    Max
  • Hi Max-san,

    Thank you for your prompt reply.

    I understand. Thank you very much.

    Regards,

    Kanemaru