Part Number: TMDS181
Hi Sirs,
Sorry to bother you.
We use TMDS181 and need confirm somethings as below.
1. We use 6.81k resistor on Pin22 VSADJ, It's Ok? Because the datasheet is use 7.96K but we don't have this value resistor. have any risk?
2. Could we float OE pin? Because from datasheet 9.2 Typical Applications, looks OE is option pin. how could we do on this pin is best??
3. Could we disconnect between I2C and GPU& SCALAR?
4. When will to use I2C?
5. There have pull high 5v on reference schematic, this 5v is for HDMI CONNECTOR or System?
Like if HDMI in have independent 5V_HDMI_IN. the SCL_SNK is 5V_HDMI_IN?
Thanks for your reading and reply.