Part Number: BQ24392
Sir/Madam,
I used part number BQ24392 dual SPST USB 2.0 high speed switch for switching as a device type dedicated charging port (DCP) where DM_CON and DP_CON are shorted to work as charge with full current mode but while testing the BQ24392 by connecting Tablet it is found that it is in slow charing mode with 410ma but the tablet requires 800ma to work in a full current mode.
I have other doubt from Datasheet of BQ24392 to make the device to be operated in charging downstream portDP_CON to be pulled down through R to GND and DM_CON connect to VDM_SRC what do mean by VDM_SRC and how much is its voltage.
Please solve the issue as early as possible.