Part Number: DP83867IR
Tool/software: Linux
I couldn't find the DP83867 Linux device driver for 3.4.39.
So I'm modifying the latest to kernel version 3.4.39.
But the ping is not working... Can I get any hints..??
/*
* Driver for the Texas Instruments DP83867 PHY
*
* Copyright (C) 2015 Texas Instruments Inc.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License as published by
* the Free Software Foundation; either version 2 of the License.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*/
#include <linux/ethtool.h>
#include <linux/kernel.h>
#include <linux/mii.h>
#include <linux/module.h>
#include <linux/phy.h>
#define DP83867_PHY_ID 0x2000a231
#define DP83867_DEVADDR 0x1f
#define MII_DP83867_PHYCTRL 0x10
#define MII_DP83867_MICR 0x12
#define MII_DP83867_ISR 0x13
#define DP83867_CTRL 0x1f
/* Extended Registers */
#define DP83867_RGMIICTL 0x0032
#define DP83867_RGMIIDCTL 0x0086
#define DP83867_SW_RESET BIT(15)
#define DP83867_SW_RESTART BIT(14)
/* MICR Interrupt bits */
#define MII_DP83867_MICR_AN_ERR_INT_EN BIT(15)
#define MII_DP83867_MICR_SPEED_CHNG_INT_EN BIT(14)
#define MII_DP83867_MICR_DUP_MODE_CHNG_INT_EN BIT(13)
#define MII_DP83867_MICR_PAGE_RXD_INT_EN BIT(12)
#define MII_DP83867_MICR_AUTONEG_COMP_INT_EN BIT(11)
#define MII_DP83867_MICR_LINK_STS_CHNG_INT_EN BIT(10)
#define MII_DP83867_MICR_FALSE_CARRIER_INT_EN BIT(8)
#define MII_DP83867_MICR_SLEEP_MODE_CHNG_INT_EN BIT(4)
#define MII_DP83867_MICR_WOL_INT_EN BIT(3)
#define MII_DP83867_MICR_XGMII_ERR_INT_EN BIT(2)
#define MII_DP83867_MICR_POL_CHNG_INT_EN BIT(1)
#define MII_DP83867_MICR_JABBER_INT_EN BIT(0)
/* RGMIICTL bits */
#define DP83867_RGMII_TX_CLK_DELAY_EN BIT(1)
#define DP83867_RGMII_RX_CLK_DELAY_EN BIT(0)
/* PHY CTRL bits */
#define DP83867_PHYCR_FIFO_DEPTH_SHIFT 14
#define DP83867_PHYCR_FIFO_DEPTH_3_B_NIB 0x00
#define DP83867_PHYCR_FIFO_DEPTH_4_B_NIB 0x01
#define DP83867_PHYCR_FIFO_DEPTH_6_B_NIB 0x02
#define DP83867_PHYCR_FIFO_DEPTH_8_B_NIB 0x03
/* RGMIIDCTL bits */
#define DP83867_RGMII_RX_CLK_DELAY_SHIFT 4
enum {
DP83867_RGMIIDCTL_250_PS,
DP83867_RGMIIDCTL_500_PS,
DP83867_RGMIIDCTL_750_PS,
DP83867_RGMIIDCTL_1_NS,
DP83867_RGMIIDCTL_1_25_NS,
DP83867_RGMIIDCTL_1_50_NS,
DP83867_RGMIIDCTL_1_75_NS,
DP83867_RGMIIDCTL_2_00_NS,
DP83867_RGMIIDCTL_2_25_NS,
DP83867_RGMIIDCTL_2_50_NS,
DP83867_RGMIIDCTL_2_75_NS,
DP83867_RGMIIDCTL_3_00_NS,
DP83867_RGMIIDCTL_3_25_NS,
DP83867_RGMIIDCTL_3_50_NS,
DP83867_RGMIIDCTL_3_75_NS,
DP83867_RGMIIDCTL_4_00_NS,
};
int rx_tx_delay = (DP83867_RGMIIDCTL_2_75_NS << DP83867_RGMII_RX_CLK_DELAY_SHIFT) | DP83867_RGMIIDCTL_2_25_NS;
module_param(rx_tx_delay, int, 0664);
static int dp83867_ack_interrupt(struct phy_device *phydev)
{
int err = phy_read(phydev, MII_DP83867_ISR);
if (err < 0)
return err;
return 0;
}
static int dp83867_config_intr(struct phy_device *phydev)
{
int micr_status;
if (phydev->interrupts == PHY_INTERRUPT_ENABLED) {
micr_status = phy_read(phydev, MII_DP83867_MICR);
printk("____%s, %d\n", __func__,__LINE__);
if (micr_status < 0)
{
return micr_status;
}
micr_status |=
(MII_DP83867_MICR_AN_ERR_INT_EN |
MII_DP83867_MICR_SPEED_CHNG_INT_EN |
MII_DP83867_MICR_DUP_MODE_CHNG_INT_EN |
MII_DP83867_MICR_SLEEP_MODE_CHNG_INT_EN);
return phy_write(phydev, MII_DP83867_MICR, micr_status);
}
micr_status = 0x0;
return phy_write(phydev, MII_DP83867_MICR, micr_status);
}
static int phy_read_mmd_indirect(struct phy_device *phydev, int prtad, int devad)
{
int value;
mdiobus_write(phydev->bus, phydev->addr, 0x0d, devad);
mdiobus_write(phydev->bus, phydev->addr, 0x0e, prtad);
mdiobus_write(phydev->bus, phydev->addr, 0x0d, (devad|0x4000));
value = phy_read(phydev, 0x0e);
return value;
}
void phy_write_mmd_indirect(struct phy_device *phydev, int prtad, int devad, unsigned int data)
{
mdiobus_write(phydev->bus, phydev->addr, 0x0d, devad);
mdiobus_write(phydev->bus, phydev->addr, 0x0e, prtad);
mdiobus_write(phydev->bus, phydev->addr, 0x0d, (devad|0x4000));
phy_write(phydev, 0x0e, data);
}
static int dp83867_config_init(struct phy_device *phydev)
{
int val;
if ((phydev->interface >= PHY_INTERFACE_MODE_RGMII) ||
(phydev->interface <= PHY_INTERFACE_MODE_RGMII_TXID))
phy_write(phydev, MII_DP83867_PHYCTRL,
(DP83867_PHYCR_FIFO_DEPTH_4_B_NIB << DP83867_PHYCR_FIFO_DEPTH_SHIFT));
if ((phydev->interface >= PHY_INTERFACE_MODE_RGMII_ID) ||
(phydev->interface <= PHY_INTERFACE_MODE_RGMII_RXID)) {
val = phy_read_mmd_indirect(phydev, DP83867_RGMIICTL,
DP83867_DEVADDR);
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_ID)
val |= (DP83867_RGMII_TX_CLK_DELAY_EN | DP83867_RGMII_RX_CLK_DELAY_EN);
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_TXID)
val |= DP83867_RGMII_TX_CLK_DELAY_EN;
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_RXID)
val |= DP83867_RGMII_RX_CLK_DELAY_EN;
phy_write_mmd_indirect(phydev, DP83867_RGMIICTL,
DP83867_DEVADDR, val);
phy_write_mmd_indirect(phydev, DP83867_RGMIIDCTL,
DP83867_DEVADDR, rx_tx_delay);
}
phy_start_interrupts(phydev);
return 0;
}
static int dp83867_phy_reset(struct phy_device *phydev)
{
int err;
err = phy_write(phydev, DP83867_CTRL, DP83867_SW_RESET);
if (err < 0)
return err;
err = dp83867_config_init(phydev);
return err;
}
static struct phy_driver dp83867_driver = {
.phy_id = DP83867_PHY_ID,
.name = "TI DP83867",
.phy_id_mask = 0xfffffff0,
.features = PHY_GBIT_FEATURES,
.flags = PHY_HAS_INTERRUPT,
.config_init = dp83867_config_init,
#if 0
.soft_reset = dp83867_phy_reset,
#endif
/* IRQ related */
.ack_interrupt = dp83867_ack_interrupt,
.config_intr = dp83867_config_intr,
.config_aneg = genphy_config_aneg,
.read_status = genphy_read_status,
.suspend = genphy_suspend,
.resume = genphy_resume,
.driver = {.owner = THIS_MODULE,}
};
static int __init dp83867_init(void)
{
printk("____%s @ %s\n", __func__,__FILE__);
return phy_driver_register(&dp83867_driver);
}
static void __exit dp83867_exit(void)
{
phy_driver_unregister(&dp83867_driver);
}
module_init(dp83867_init);
module_exit(dp83867_exit);
static struct mdio_device_id __maybe_unused dp83867_tbl[] = {
{ DP83867_PHY_ID, 0xfffffff0 },
{ }
};
MODULE_DEVICE_TABLE(mdio, dp83867_tbl);
MODULE_DESCRIPTION("Texas Instruments DP83867 PHY driver");
MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com");
MODULE_LICENSE("GPL");