This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

what is the Difference between MAC mode and PHY mode

I'm having an Ethernet switch . It's a 3-way switch but only has 2 integrated PHYs and for the 3rd port it has an RMII interface.

Datasheet says that the 3rd port can work in 'MII MAC mode' or 'MII PHY mode'. On power on the default is 'MII PHY mode

Which mode do I need to use to connect an external PHY?