Part Number: TPS65982-EVM
Hi,
I have two of these devices (TPS65982-EVM), one device seems to be defective. I am using two devices to test: a mobile phone with USB-C port and the second TPS65982-EVM. Using a known-good USB-C cable, one device can sync up/enumerate the PDO, however, the other TPS65982-EVM can only detect and enumerate if I change the cable orientation.
Troubleshooting done:
DIP switch on both TPS65982-EVM at 0110 (Config 6) using Dell 20v / 3a power adapter
1. Using a phone with native USB-C (only one sink PDO, 5v/1.5a), with both TPS65982-EVM configured exactly the same, one TPS65982-EVM will only enumerate with one cable orientation and will not enumerate if cable is reversed. The other TPS65982-EVM will work no matter the orientation of USB C.
DIP switch on both TPS65982-EVM 0000 (Config 0), one using Dell 20v/3a power adapter
1. TPS65982-EVM will only sync up, if the cable is properly oriented on the defective TPS65982-EVM
Kindly assist...