This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AN-917 states RS232 to RJ45 pin outs



Pin 8 is Request to Send/Ready for Receiving which means RTS or DSR . Do you have any system design with such functionality using 8 line for modems connections. As i have seen on other blogs RI and DSR is merged as RI is used for dial up modems alone.

  • Hi Anusha,

    RI and DSR generally have different functions, so it isn't clear to me how they could be merged. If you do not plan to connect to a dial-up modem, it may make sense to just leave RI disconnected instead since there will be no need for ring indication. (Even if a dial-up modem is used, you may be able to avoid using RI and instead use the other data lines to communicate the modem status to your DTE.)

    I may be misunderstanding your question, though - if so, please let me know.

    Regards,
    Max