This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822H: RGMII connection to MCU. Recomended magnetics and ESD protection diodes.

Part Number: DP83822H


I'm using this IC with AM335X MCU, in RGMII mode.

In DP83822 datasheet COL/GPIO2 pin have this description:

"Collision Detect: For Full-Duplex mode, this pin is always LOW. In HalfDuplex mode, this pin is asserted HIGH only when both transmit and receive media are non-idle.
Unused in RMII Mode"

But AM335X family doesn't have RGMII_COL pin. Am I correctly understood that doesnt used in RGMII mode too?

And second question: what magnetics and ESD protection diodes are recomended for application? May be you have an AppNote for that?
Best regads.

  • Hi Nikita,

    You are correct that COL is not used for RGMII. I should have added a comment for it when I wrote the DS. The next page though (page #6) I do explain that COL can be used as a GPIO when in RGMII operation.

    At the bottom of the DS I list recommended magnetic parameters if you would like to pick a transformer and I also listed magnetics I have tested in lab.

    The EVM has the recommended TVS array. The part number for this will be in the schematic PDF.

    Kind regards,
    Ross
  • Oh, sorry you are right. That's my inattention. TY, for adressing to EVM board, that's really useful information.