Part Number: SN65CML100
Other Parts Discussed in Thread: DS90LV011A
Can the Vbb reference voltage be used to interface the input of the SN65CML100 to a 3.3V LVCMOS single-ended input? The data sheet describes a single-ended PECL interface, but maybe this would work with a CMOS type driver. The minimum Vih of the input signal would be 2.0V, which seems to give enough differential input margin to the SN65CML100 inputs. Vil would be < 0.8V.
Signalling rate is 20 MHz.
Any concerns with such an interface?