Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2511: Erroneous values on the D+/D- signals

Part Number: TPS2511

We are using the TPS2511 for a dedicated charging port for a certified USB device.  In 2015 the device passed USB DCP certifications without issue, subsequent testing with the same design in 2017 yielded failures on multiple protocols including: resistance between D+ and D-, and both primary/secondary detection of D+/D- (supposed to be 0.6V nominal).  The design we inherited contains only a common mode choke on the D+/D- lines and some low capacitance ESD diodes.  What would cause the TPS2511 from providing erroneous values on the D+/D- signals using identical circuits?  The date codes on the TPS2511’s are 4A and 61.

Thanks,

Vichet