Part Number: SN65DSI85-Q1
Hi,
Let me confirm about below.
--
According to datasheet, in case of "LEFT/RIGHT mode", I understand that there is limitation for sync size.
"Neither the channel A LEFT portion input or the channel B RIGHT portion input per line shall exceed 1408 pixels, which is defined as ½ of the
maximum line size (2560 pixels in WQXGA 2560x1600 mode) plus 10% headroom."
(Please see 8.3.5 DSI Video Transmission Specifications about detail)
Then, I want you to confirm whether there is also limitation for sync size in case of "Single-channel DSI to single-channel LVDS mode" or not ?
Customer want to input/output following resolution.
* 720x1920 (Not 1920x720)
In case of "LEFT/RIGHT mode", this case is not available, but I also want you to confirm whether there is setting that above resolution is available or not.
Best Regards,
Machida