Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848Q-Q1: DP83848Q-Q1 RMII External Reference Clock

Part Number: DP83848Q-Q1

I have a customer that is interested in using an external oscillator for RMII and using it to provide a clock to both the PHY and the MAC.

How should the external oscillator be selected, if it's being used to supply the clock to both the PHY and the MAC (Load Capacitance)?

How should these signals be routed in layout to maximize the signal integrity?

-Joe

  • Hi Joe,

    What is the setup and hold time of the MAC you are using?
    Also, what is the delay in relation to the reference clock of the MAC you are using?
    The DP83848Q timing is listed in the datasheet. With about 1ns/6inch of prop delay for FR4, we can figure out the best place to locate the oscillator.
    Also, as for load capacitance, the interface is spec'd to 25pF.

    Kind regards,
    Ross