Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2077A: USB compliance test packet downstream port

Part Number: TUSB2077A

Hi

Could you please support following questions?

Q1 : Is TUSB2077A possible to output the test packet for the compliance test?

        Also is it possible to select the each downstream port for that test?

 

Q2 : If Q1 is possible, could you provide the sample program (/or script) for the above test?

Q3 : If there are no sample program , could you give us the register setting for that configuration?

Thanks

Muk