Other Parts Discussed in Thread: TSU6111
Hi,
This is a general usb question and was wondering if TI would have any products to solve the issue. Basically I'm looking for a way to charge the USB host in a USB-OTG setup. Basically I have a camera which has support for external USB mic. I want to use the external MIC and charge at the same time using a power bank. The camera has to support OTG since it' acting as the host when the mic is connected and as a slave device when connected to a computer for data transfer. On lots of googling, I came across Accessory Charging Adapter which let's you charge the host device in an OTG setup. As far as I understand it is basically inserting a resistor between the ID pin and GND instead of direct connection to GND. But I couldn't find any such adapter I can buy on the web. So I was wondering if TI would have any solutions using which I could build one on my own. I'm also aware that even if I get the hardware right, the software on the cam might not allow what I'm trying to do.
So basically, I'm trying to use a USB microphone and charge the cam at the same time.
Edit: After a bit of searching and reading USB battery charging spec 1.2 I came to understand that Accessory Charging Adapter is what I need. Does TI have any products to do the same.
Thanks and Regards.