Part Number: TPS65981
Other Parts Discussed in Thread: DP-EXPANSION-EVM, , , HD3SS460
Hello Team,
Could you please answer my customer question,
We are now evaluating the TPS65981 Type C PD controller on the TPS6598EVM + DP-EXPANSION-EVM, running the TPS6598x Application Customization Tool.
Our requirements are:
- the TPS6598EVM is power source up to 100W
- an USB 3.0 device is connected to the TPS6598EVM using the DP-EXPANSION-EVM module. This data will be upstreaming to a host (UPF).
so, our hardware (using the TPS65981) should be able to power a host (e.g. notebook) and upstream one USB SuperSpeed port to this host.
I tested the TPS65981EVM in the default docking station mode with an external power supply (170W), set to 20V and 5A (OCP).
I did not change any settings from defaults..
Unfortunately the system is quite unstable (sometimes works, sometimes not...).
Is there a special firmware for our needs available or can you give us some parameter setting advice?
Thank you very much.
Best Regards,
Needhu