Part Number: TUSB8041
Other Parts Discussed in Thread: TUSB8041
Hello,
I have 4 fold question;
1. Do you have a default file for configuring the EEPROM, so I only have to change the parts I need, and the rest are as default (i.e the registers if no EEPROM attached). This is because the “reset” function in the software simply sets it all to “FF” not the default from inside the usb hub.
2. Is there a command line utility to automate the programming?
3. If I write “55” to address 0x00 it will use th EEPROM. But from reading the document with the software, you can then not wipe or reconfigure the EEPROM from the software? Is this correct?! If so, how do I wipe the EEPROM if we need to configure it differently after programming? (.e. SMD devices we don’t want to be removing just to reconfigure them!)
4. Furthermore, the recommendation in the TUSB8041 data sheet USB-B upstream port and the implementation on the evaluation board do not match:The datasheet shows as below. However, this does not flow without swapping the P/M lines. This appears (after continuity checking) on the evaluation board.
Is there a reason that this has been intentionally avoided? Which is the best practice
Will appreciate responses on this