Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI: USB HUB drawing too much current, not responsive

Part Number: TUSB4020BI

Hello,

I have a TI USB Hub on a pcb that is drawing 150 mA of current on the 1.1V rail before the 3.3V rail is on, and around 230 mA when the 3.3V rail is on.  The datasheet states a current draw around 80 mA.  The device does not appear to be working as my upstream PC does not recognize the PCB when plugged in.  However, I have traced out all the pins without finding any problems.  Any suggestions?