Part Number: TUSB8044RGCEVM
Hi
Is the TUSB8044RGCEVM can switch the ports on demand using some software or command? If yes, wich software need to use?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB8044RGCEVM
Hi
Is the TUSB8044RGCEVM can switch the ports on demand using some software or command? If yes, wich software need to use?
Thank you
For example, I have one PC connected with 4 cellphones, but I just want to connect with one cellphone, so I need to turn off (VBUS and data) of other 3 connections by command using this same PC.
Do you think is easy to do? ("modify the USB Driver on your PC in order to send the "power off" (and "power on")")