Part Number: TPS65982
Hello experts,
I am using the TPS65982 for a type C controller and in a few systems (50%) I am not able to get an ack from the part when the address 0x38 is on the I2C bus. The TPS is acting as a slave with address 0x38...what could cause the TPS not to ack the address?
I am using the primary I2C interface, the part is not in reset and power is good.
Would having a corrupt PROM image cause issues and inhibit the TPS to ACK?
How close to 100kHz does my SCK frequency have to be. My clock is about 9.2us or about 110KHz.
Regards,
Guy