Part Number: HD3SS6126EVM
Other Parts Discussed in Thread: HD3SS3220, TIDA-00891, HD3SS2522
Hi
I want a USB multiplexer to help me achieve the following:
2 USB inputs to the multiplexer
Input 1- From a regular android wall charger (will convert the C type output to the required USB-A type using a female C-type to USB-A adapter)
Input 2 - USB output from the PC (will again use an adapter to connect to the USB input of the multiplexer)
Output - Should be able to select between Output 1/2 and route it to the phone that will be connected to the output
The main criteria is that when I am routing from input 1 to the phone, the multiplexer should be able to route the 3A charging current to the phone.
Will the HD3SS6126EVM help me do that?
Thanks
Srinivas