Part Number: DS90UB954-Q1
Hello ,
We are trying to interface DS90UB954 Deserializer with R-car H3. The problem we are facing is that Renesas board has QSH-030-01-L-D-A connector on its module. So what we find difficult is to interface this Deser with Renesas. So we are looking for either an Deserializer board which has QSH-030-01-L-D-A connector , or an interface board(Daughter card) which has QSH-030-01-L-D-A connector and DS90UB954 presenrt in it. So any solution might be better to conclude . Is there a possibility to find a Deserailizer board directly which will have QSH-030-01-L-D-A connector , so that it will be compatible with R car H3 . If not , at least any daughter board that has support for this Deserailizer which has the same connector , so that it can be connected to H3 board
Regards,
Aravind S