Part Number: DS90UB964-Q1
Hi,
I buit a OV2775+953-->964 system for a SVS applicaton, when camera module is connected to 964 RX0 port, sensor ID can be detected but when sensor setram on, ID sometimes can not be detected.
If I move the move connected to RX1 port, sensor ID can not be detected.
When sensor stream on, there will be a large current, so I provided an independent power5~12v on 964 side, but still no improvement with ID detection.
I guess the BCC communication is not good, but I have no idea how to established a stable BCC, could you provide some suggestions
BTW,
What is the main difference between 964 and 960?
I have a 964 board which is good with 913
If used it with 953, HW need to be modified or not? Just change 964 and 953 init setting?