Other Parts Discussed in Thread: USB-CTM-MINIDK-EVM
Hi,
Please let me ask the case of the operation with VCM=0V. From the USB specification, the differential voltage pp is 1.2V diff pp so the negative swing will be -0.3V when VCM=0V. I believe that it will not damage to HD3SS3212 because abs max of Differential I/O is -0.5V. but then I'd like to know if you can guarantee to use with this condition.
Please let me know if you need more information.
Best Regards,
Satoshi / Japan Disty