This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3220: HD3SS3220 Mux problem

Part Number: HD3SS3220

Hi!

We use HD3SS3220 in our design and have some problem with USB 3.0 interface muxing. HD3SS3220 configured in DFP mode and when attached the usb cable with flash drive (the cable is USB Type-C to USB 3.1 Standard-A Receptacle Adapter), but USB 3.0 interface works only in one orientation position of USB C plug. CC1 and CC2 pins has 0.4V and 4.8V levels depends on cable's orientation when it is attached, but DIR pin always in high level. We tryed to use 4.7K PU on DIR pin, but nothing helps.  When we manually set DIR pin to GND, the switch works with another cable orientation, so i think, that layout is ok. I tryed to disconnect the HD3SS3220 from I2C bus, but no result. Can we use switch without connection to I2c bus? Can you help us with this problem?