This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK10232: HS_RX register setting optimization procedure

Guru 19785 points

Part Number: TLK10232

Hello Team,

Thank you for the register explanation material in following URL.

https://e2e.ti.com/support/interface/high_speed_interface/f/138/t/595706

Since our customer observes errors at HS_RX side, they are trying to optimize the HS_RX register settings. They do not use link training (manual setting).

There are too many parameters and combinations to be optimized for the HS_RX register settings in Address 0x1E, 0x0004 register.

What is the best procedure, step by step, to optimize each settings ? (1st optimize xxx, then yyyy....)

And how can we judge if that setting is optimized or not ?

We would appreciate it if you could explain us in specific.

Best Regards,

Kawai

  • Hi Kawai,

    The RX SERDES settings must still need some type of adjustment. This is where you have to spend time tuning those settings until it's (mostly) error free.
    HS_SERDES_CONTROL_1/2/3 (not 4 since that's pre-emphasis, only for copper links not optical)

    Focus first on:
    HS_ENTRACK
    HS_EQPRE
    HS_PEAK_DISABLE
    HS_H1CDRMODE

    Through HS_ERROR_COUNTER user is able to verify the number of invalid code words. As well monitor CHANNEL_STATUS_1 to verify the link status.

    Best Regards,
    Luis
  • Hi Luis-san,

    Thank you for your support and I apologize for my delay.

    I understood that first you should focus on the four parameters (HS_ENTRACK, HS_EQPRE, HS_PEAK_DISABLE, HS_H1CDRMODE), however, do we need to check all the register value combination one by one to check the errors ?

    Normally, equalizer gain should be optimized based on trace length, however, I thought the result may differs by other register value in combination (might also depend on optical modules).

    After optimizing the above 4 registers, there are other parameters to look into.
    When these changed, do we need further optimization including the above 4 registers ?

    Best Regards,
    Kawai
  • Hello Kawai,

    Unfortunately when the link training is not enabled the process to adjust the RX settings is a little exhaustive. The user needs to try different combinations to avoid bit errors.

    Attached you will find an application note with a explanation of these parameters to tune the device according every system.

    I hope this helps.

    TLK10034_link_training_app_note (10).doc

    Best Regards,

    Luis Omar Moran

    High Speed Interface

    SWAT Team

  • Hi Luis-san,

    Thanks for your continuous support.

    Best Regards,
    Kawai