Part Number: ISO5852S
Hello. Problem: the level of operation of the overcurrent protection of the 9 Volt(DESAT pin). How can it be regulated by external components? For example, I have a 600V / 100A transistor, permissible 200A. I want to configure the driver at 400 A. This corresponds to ~ 2V drop on the IGBT transistor. I do not want to type a long chain of fast diodes. Are there alternatives?