This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2549-Q1: Question about USB Charge supporting 2.4A(DividerMode3)

Genius 4260 points

Part Number: TPS2549-Q1
Other Parts Discussed in Thread: TPD2S703-Q1, , TPS254900-Q1, TPS2514A, TPS2549, TPS2513

Hi,

If I'd like to realize USB Charge supporting following conditions,

1.  charge current up to 2.4A (Divider mode 3)

2. Short-to-Battery (up to 18 V) and Short-to-VBUS protection on VD+, VD–

Can these two conbinations of ICs support them?

#1 TPS2549-Q1 + TPD2S703-Q1

#2 TPS254900-Q1 + TPS2513-Q1

If they have any problem , pelase let me know.

Thanks

Go