Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90LV804: DS90LV804 4ch Sub-LVDS Repeater usage

Part Number: DS90LV804
Other Parts Discussed in Thread: DS10BR150,

Dear Engineers

I'd like to use two DS90LV804 and one DS10BR150 as 8-ch sub-LVDS Repeater like below block diagram.

Let me know this is possible connection (Maximum data rate for each lane is less than 800Mbps)

Thanks In Advance

Hennessy

  • Hennessy,

    It is possible to use this combination of devices.  I would caution you that the typical propagation delay through the DS10BR150 is much faster than the DS90LV804.  If the interface cannot handle this difference in skew between the clock and data, the circuit may not work as intended.

    You may want to substitute another device for the DS90LV804 or use 3 DS90LV804's to keep the propagation delays equal.

    Regards,

    Lee