Part Number: DP83822I
Hi,
I have a question about DP83822I.
I'm searching magnetics which can be used with DP83822I.
I'm planning to use H1102FNL.
This magnetic specfication doesn't meet the recommended transformer specification
which are written at DP83822I datasheet page.100 "Table 137 Transformer Electrical Specification".
It doesn't meet the spec only a little, but will it cause any problem?
pdf1.alldatasheet.com/.../H1102FNL.html
In DP83822I datasheet, there are recommended transformer product listed at Table 136.
We also searching RJ45 connector which include transformer and there no list in datasheet.
Are there any recommended RJ45 connector(include transformer) for DP83822I?
If the transformer in RJ45 connector meets above "Table 137 Transformer Electrical Specification",
can it be used with DP83822I without any problem?
best regards,
g.f.