Part Number: TUSB3210
Dear Mr.,Mrs.
I use the TUSB3210 for USB-to-GPIO application.
I have already received the TUSB3210KBDFW sample source from TI.
My TUSB3210 firmware was confirmed running well by checking Debug uart and the USB HID driver in windows was attached well (in device manager of windows 7).
(my firmware have 2 end-point for input & output.)
I made the C# application in windows 7 for control the device but I can't communicate to board.
Any information about the method of communication to USB HID TUSB3210 board in Windows is it?
Any check information whether the USB HID device is attached well in windows or not?
Thanks
Cheolhyeon Cho