Part Number: DS110DF410
Hi,
I wanted to confirm the register settings for 10GE. I understand the steps as follows.Is my understanding correct?
|
Step |
Shared/Channel Register Set |
Operation |
Register Address (HEX) |
write value (HEX) |
Comment |
|
1 |
Share |
Write |
FF |
0C |
Write all channels |
|
2 |
Channel |
Write |
0A |
1C |
Assert CDR reset |
|
3 |
Channel |
Write |
15 |
10 |
Set DEM(default,change as needed) |
|
4 |
Channel |
Write |
31 |
20 |
Set Adapt Mode 1(Default) |
|
5 |
Channel |
Write |
1E |
E9 |
Disable the DFE since most application do not need it(Default) |
|
6 |
Channel |
Write |
2D |
80 |
Set VOD value(Default,change as needed) |
|
7 |
Channel |
Write |
2F |
06 |
Ethernet(Default) |
|
8 |
Channel |
Write |
0A |
10 |
Release CDR reset |
Best Regards,
Toshiyuki