This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LCD Segment Driver

Guru 20090 points


Hello,

Are there any line up of LCD segment driver?
Competitor example is BU91796MUF.
In the cross reference result, I jump the Interface page. Thus I post this question to this forum.

Specifications are the following

1/4 duty, 60 segment, Automotive qualified, Vin:2.7~5.5V

Best Regards,
Ryuji