Part Number: SN65DSI86EVM
Other Parts Discussed in Thread: SN65DSI86
Hi,
I am currently using a SN65DSI86EVM board to evaluate using this DSI to DP converter IC for use driving an embedded LCD screen. Currently, I am using a LCD driver board with an HDMI input for initial prototype testing, but intending to drive the LCD directly from the SN65DSI86 IC in the future.
I am trying to get the DP output to display the color bars from the IC to test the DP output, and then will be working to solve my DSI input configuration if there is any issues. I am getting LT_FAIL flag in register 0xF8 (value is 0x02), but am unable to figure out why that is happening. I have used the example from the EVM user guide, as well as going through the scripts posted here (e2e.ti.com/.../2062378) to try to configure the output, but no avail at all.
Any help with debugging this would be appreciated.
Regards,
John Basista