This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH948-Q1: Default register value for Port 1

Part Number: DS90UH948-Q1

Hi,

I would like you to confirm about default value of Port 1 register.

According to datasheet, some registers of DS90UH948 should be set Port 0 and Port 1 individually depending on usecase.

I understood that default value of these registers for Port0 and Port1 are same because there is no desciption about default value for port 1 especially.

However, when I checked the default value when I set 0x34[1:0] to 0b11, I observed un-expected value for folloing register.

1. When 0x34[1:0]=0b01, (Read value is for Port 0)
0x1D 0x10
0x1E 0x00
0x1F 0x00
0x56 0x00

2. When 0x34[1:0]=0b11, (Read value is for Port 1)
0x1D 0x13
0x1E 0x33
0x1F 0x03
0x56 0x08

I expected that I can see same value for above "2".
However, the result was different.

So could you please confirm about default register value for Port 1 ?

Best regards,

Machida